Returns the low-order 16-bit value of a term.
[Function]
Returns the value of the lower-order 16 bits among the 32 bits of a term.
[Application example]
MOVW AX, #LOWW(0x12345678) ; (1)
|
(1) | By executing a MOVW instruction, this operator loads the low-order 16-bit value "0x5678" of the expression "0x12345678" to AX register. |