Everything

.DBIT


Allocates a bit area of one bit.

[Syntax]

Symbol field
Mnemonic field
Operand field
Comment field
[name]
.DBIT
 
[; comment]

[Function]

-

Allocates a bit area of one bit.

[Description]

-

This directive can be written in only a bit section.

-

This directive is used to allocate a bit area of one bit in a bit section.

-

The contents of the allocated bit area are undefined.

-

When a name is written in the symbol field, it will be defined as a bit symbol which has an address and bit location as its value.

[Example]

        .BSEG
BSYM1   .DBIT   ; Bit area of one bit is allocated
        .DBIT   ; Bit area of one bit is allocated
BSYM2   .DBIT   ; Bit area of one bit is allocated
        .CSEG
        SET1    BSYM1
        CLR1    BSYM2