Converts a character string to an integer (uintmax_t type) and stores the pointer to the last character string.
uintmax_t __far strtoumax(const char __near * restrict nptr, char __near * __near * restrict endptr, int base); (C99)
uintmax_t __far _COM_strtoumax_ff(const char __far * restrict nptr, char __far * __far * restrict endptr, int base); (C99)
If the partial character string has been converted, the converted value is returned. If the character string could not be converted, 0 is returned.
If an overflow occurs, this function returns UINTMAX_MAX and sets macro ERANGE to global variable errno.
This function skips 0 or more columns of white-space characters (character which makes the isspace function true) from the start of the string indicated by nptr, and converts the string from the next character into a uintmax_t-type representation. If base is 0, the string is interpreted as the C radix representation. If base is in the range from 2 to 36, the string is interpreted as a radix. When endptr is not a null pointer, the pointer to the remaining strings that were not converted is set in endptr.