Obtain absolute value (int type)
Returns the absolute value of j (size of j), | j |. If the input value of abs is the smallest negative value, the same value is returned.
This function obtains the absolute value of j (size of j), | j |. If j is a negative number, the result is the reversal of j. If j is not negative, the result is j.