11.4.6 Error output regarding an address not in the saddr access range
When the -dev option is specified, an error will be output for an address outside of the saddr access range. However, an error will not be output when the -dev option is not specified.
Example | >ccrl -cpu=S3 file.asm -lnkopt=-start=.text/100,.bss/f9f34 |
mov a,!sym
mov a,sym ; When the -dev option is specified, an error will be output.
.section .bss, bss
sym: .DS (1)
|