< Assembler Command Options / Object Options >
When the CPU*1 is selected or RXv1 or RXv2 is selected as ISA*2, -nobank is assumed to be specified.
In other cases, -bank is assumed to be specified.
*1) This means a selection by the cpu option or the CPU_RX environment variable.
*2) This means a selection by the isa option or the ISA_RX environment variable.
This option enables writing of the SAVE and RSTR instructions dedicated to the register bank save function. |