Everything

-binary


< Optimizing Linkage Editor (rlink) Options / Input Options >

[Format]

-binary = <suboption>[,...]
          <suboption>: <file name>(<section name>
                         [:<boundary alignment>][/<section attribute>][,<symbol name>])
          <section attribute>: CODE | DATA
          <boundary alignment>: 1 | 2 | 4 | 8 | 16 | 32 (default: 1)

[Description]

-

Specifies an input binary file. Two or more files can be specified by separating them with a comma (,).

-

If an extension is omitted for the file name specification, bin is assumed.

-

Input binary data is allocated as the specified section data. The section address is specified with the start option. That section cannot be omitted.

-

When a symbol is specified, the file can be linked as a defined symbol. For a variable name referenced by a C/C++ program, add an underscore (_) at the head of the reference name in the program.

-

The section specified with this option can have its section attribute and boundary alignment specified.

-

CODE or DATA can be specified for the section attribute.

-

When section attribute specification is omitted, the write, read, and execute attributes are all enabled by default.

-

A boundary alignment value can be specified for the section specified by this option. A power of 2 can be specified for the boundary alignment; no other values should be specified.

-

When the boundary alignment specification is omitted, 1 is used as the default.

[Examples]

input=a.obj
start=P,D*/200
binary=b.bin(D1bin),c.bin(D2bin:4,_datab)
form=absolute

-

Allocates b.bin from 0x200 as the D1bin section.

-

Allocates c.bin after D1bin as the D2bin section (with boundary alignment = 4).

-

Links c.bin data as the defined symbol _datab.

[Remarks]

-

When form={object | library} or strip is specified, this option is unavailable.

-

If no input object file is specified, this option cannot be specified.