Everything

-section_forbid


< Optimizing Linkage Editor (rlink) Options / Optimize Options >

[Format]

-section_forbid  = <sub>[,...]
                   <sub>: [<file name>|<module name>](<section name>[,...])

[Description]

-

Disables optimization for the specified section. If an input file name or library module name is also specified, the optimization can be disabled for a specific file, not only the entire section.

[Remarks]

-

If optimization is not applied at linkage, this option is ignored.

-

To disable optimization for an input file with its path name, type the path with the file name when specifying section_forbid.