Everything
3.1.1 Source Information

The source information is included in the object information when the -show=source option is specified. For an example of source information, refer to the next section, Object Information.