Everything
3.3.2 Option Information

The option strings specified by a command line or a subcommand file are output.

The following figure shows an example of option information output when rlink -subcommand = test.sub -list -show is specified.

Item Number

Description

(1)

Outputs option strings specified by a command line or a subcommand in the specified order.

(2)

Subcommand in the test.sub subcommand file.