Calculates the arc sine of a floating-point number.
f Floating-point number for which arc sine is to be computed
Abnormal: Domain error: Returns not-a-number.
A domain error occurs for a value of f not in the range [–1.0, +1.0].
The asinf function returns the arc sine in the range [–π/2, +π/2] by the radian.