Everything

strlen


Calculates the length of a string.

[Format]

#include <string.h>

size_t strlen (const char *s);

[Parameters]

s Pointer to the string to check the length of

[Return values]

Number of characters in the string

[Remarks]

The null character at the end of the s string is excluded from the string length.