Calculates the exponential function value of a complex number.
[Format]
#include <complex.h>
float complex cexpf(float complex z);
double complex cexp(double complex z);
long double complex cexpl(long double complex z);
[Parameters]
z Complex number for which exponential function is to be computed
[Return values]
Exponential function value of z