Everything
7.5 EC++ Class Libraries

This section describes the specifications of the EC++ class libraries, which can be used as standard libraries in C++ programs. The class library types and corresponding standard include files are described. The specifications of each class library are given in accordance with the library configuration.

-

Library types

Table 7.15 shows the class library types and the corresponding standard include files.

Table 7.15

Class Library Types and Corresponding Standard Include Files

Library Type

Description

Standard Include Files

Stream input/output class library

Performs input/output processing

<ios>, <streambuf>, <istream>, <ostream>, <iostream>, <iomanip>

Memory management library

Performs memory allocation and deallocation

<new>

Complex number calculation class library

Performs calculation of complex number data

<complex>

String manipulation class library

Performs string manipulation

<string>