Everything
8.2 File Contents

Startup routine that The Renesas integrated development environment (IDE) for RX Family supplies is as follows:

Table 8.1

List of Programs Created in Integrated Development Environment

 

File Name

Description

(a)

resetprg.c

Initial setting routine (reset vector function)

(b)

intprg.c

Vector function definitions

(c)

vecttbl.c

Fixed vector table*1

(d)

dbsct.c

Section initialization processing (table)

(e)

lowsrc.c

Low-level interface routine (C language part)

(f)

lowlvl.src

Low-level interface routine (assembly language part)

(g)

sbrk.c

Low-level interface routine (sbrk function)

(h)

typedefine.h

Type definition header

(i)

vect.h

Vector function header

(j)

stacksct.h

Stack size settings

(k)

lowsrc.h

Low-level interface routine (C language header)

(l)

sbrk.h

Low-level interface routine (sbrk function header)

Notes 1.

This is for the RXv1 instruction-set architecture.
For an RX instruction-set architecture other than the RXv1 instruction-set architecture, this becomes the "exception vector table".