Everything
Everything
top
Compiler
QUICK GUIDE
Reducing the Code Size
A.6
Reducing the Code Size
This section describes code size reduction.
To the latest version of this page
Differences Information
Previous Topic
Transferring Variables with Initial Values from ROM to RAM
Next Topic
Data Structure
Table of Contents
Variables (C Language)
Functions
Using Microcomputer Functions
Variables (Assembly Language)
Startup Routine
Reducing the Code Size
Data Structure
Local Variables and Global Variables
Offset for Structure Members
Allocating Bit Fields
Optimization of External Variable Accesses when the Base Register is Specified
Specified Order of Section Addresses by Optimizing Linkage Editor at Optimization of External Variable Accesses
Interrupt
High-Speed Processing
Modification of C Source