Detailed information on a Point Trace event is edited in the Detailed Settings of Point Trace dialog box. This dialog box is opened by selecting the Point Trace event you desire to edit on the Events panel then selecting [Edit Condition...] from the context menu.
The compare condition, address and address mask can be specified as an address condition in the Detailed Settings of Point Trace dialog box.
The access type, access size, compare condition, compare data and data mask can be specified as an data condition in the Detailed Settings of Point Trace dialog box.
The pass count can be specified as an pass count condition in the Detailed Settings of Point Trace dialog box.
The following can be specified as an event target in the Detailed Settings of Point Trace dialog box.