Items in the trace panel can be linked to other panels using the currently selected line address as a pointer (window focus will not move).
Click the 
 button on the toolbar to start linking to the Editor panel.  Click the 
 button on the toolbar to start linking to the Disassemble panel. 
If the button is clicked again, the link is disconnected.
The Editor panel/Disassemble panel opens when selecting the [Jump to Source]/[Jump to Disassemble] from the context menu with moving the caret to the source line/address corresponding to the address of the currently selected line (focus is moved).  |