The following types of events can be set or deleted during program execution, or during tracer/timer execution.
: Possible, if the program execution is allowed to pause for eventsNote
: Impossible while tracer or timer is executing
: Impossible while tracer or timer is executing. Possible, if the program execution is allowed to pause for eventsNote
To enable this, specify [Yes] with the [Set event by stopping execution momentarily] property in the [Set Event While Running] category on the [Debug Tool Settings] tab of the Property panel. |
: Not supported