Everything
2.10.2.1 Execute after resetting microcontroller (CPU)

Reset CPU and start execution of the program from the reset address.

Click the button on the debug toolbar.

When this operation is performed, the program continues to be executed until either of the following occurs:

 

-

The button has been clicked (see "2.11.2 Stop the program manually").

-

The PC has reached a breakpoint (see "2.11.3 Stop the program at the arbitrary position (breakpoint)").

-

Other break causes have occurred.

Remark 1.

This operation is the same as when the button is clicked after clicking the button.

Remark 2.

In cases of failure to reset, the following setting may be required to enable resetting.

-

The [Reset While Running] category on the [Debug Tool Settings] tab of the Property panel

[Use the force reset] property

[Yes]