Follow the steps below on the Download Files dialog box to download multiple load module files.
When debugging a program consisting of multiple load module files, care should be taken to avoid overlapping of location addresses. |
When the [Add] button is clicked, a blank list item "-" is displayed in the last line of the [Download file list] area.
Configure the download conditions for the download file to add in the [Download file property] area.
Configure each item displayed with the following condition.
When the configuration is completed, the file name specified in this property is displayed in the blank list of the [Download file list] area.
Specify the name of the load module file to be added (up to 259 characters). |
|||
Directly enter from the keyboard, or specify with the Select Download File dialog box opened by clicking the [...] button displayed at the right edge of this property when it is selected. |
|||
Select whether to download the object information from the specified file. |
|||
Select whether to download the symbol information from the specified fileNote 1. |
|||
Select whether to generate the information for the Symbol name completion function when downloadingNote 2. |
|||
Generates the information for the symbol name completion function. (i.e. uses the symbol name completion function.) |
|||
Does not generate the information for the symbol name completion function. (i.e. does not use the symbol name completion function.) |
If the symbol information have not been downloaded, the source level debugging cannot be performed. |
When [Yes] is selected, the time taken for downloading and the memory usage on the host machine will increase. We recommend selecting [No] in this item if you do not intend to use the symbol name completion function. |
You can decrease the memory usage by selecting [No] for the [Download symbol information] item if the symbol information is not required for the module (in this case, however, the source level debugging can not be performed for the file). |
The order of the download is the display order of the files displayed in the [Download file list] area.
If you want to change the order, use the [Up]/[Down] button.
Enable all the configuration in this dialog and add the specified load module file (the specified file name is displayed in the [Download] category on the [Download File Settings] tab of the Property panel).