2.12.5.1
Change display format of values
The display format of the [value] area can be changed using buttons below on the toolbar.
Notation
|
The following buttons to change the notation of a data value are displayed.
|
|
AutoSelect
|
Displays values on this panel in the default notation according to the type of variable (default).
|
Hexadecimal
|
Displays values on this panel in hexadecimal number.
|
Decimal
|
Displays values on this panel in decimal number.
|
Octal
|
Displays values on this panel in octal number.
|
Binary
|
Displays values on this panel in binary number.
|
Decimal Notation for Array Index
|
Displays array indexes on this panel in decimal number (default).
|
Hexadecimal Notation for Array Index
|
Displays array indexes on this panel in hexadecimal number.
|
Float
|
Displays values on this panel in float.
Note that when the value is not 4-byte data, or has the type information, displays it in the default notation.
|
Double
|
Displays values on this panel in double.
Note that when the value is not 4-byte data, or has the type information, displays it in the default notation.
|
|
Adds the value in hexadecimal number enclosing with "()" at the end of the value.
|
Encoding
|
The following buttons to change the encoding of character variables are displayed.
|
|
ASCII
|
Displays character variables in ASCII code (default).
|
Shift_JIS
|
Displays character variables in Shift-JIS code.
|
EUC-JP
|
Displays character variables in EUC-JP code.
|
UTF-8
|
Displays character variables in UTF-8 code.
|
UTF-16 Big-Endian
|
Displays character variables in UTF-16 Big-Endian code.
|
UTF-16 Little-Endian
|
Displays character variables in UTF-16 Little-Endian code.
|
UTF-32 Big-Endian
|
Displays character variables in UTF-32 Big-Endian code.
|
UTF-32 Little-Endian
|
Displays character variables in UTF-32 Little-Endian code.
|