Connect a host machine and E20. If required, connect a target board, too.
See E20 User's Manual for details on the connection method.
Figure 2.3 | Connection Example [E20] |
Caution | Only serial communications are supported as the communication method with the target board (JTAG communications is not available). |