Registered watch-expressions can be organized in categories (folders) and displayed in tree view (there is no category as default).
Up to 64 categories can be created in one watch panel (if this restriction is violated, a message appears). |
Move the caret to the position to create a new category then click the button in the toolbar and directly enter the new category name.
Click the category name to edit, and click it again, then directly modify the category name from the keyboard.
Select categories to delete then click the button in the toolbar.
Registered watch-expressions are categorized when they are dragged and dropped in the category.
Also, the display order of the categories and the watch-expressions (upper or lower position) can be changed easily by drag and drop operation.