Call stack information is displayed in the Call Stack panel below.
Select the [View] menu >> [Call Stack].
For details on the contents and function in each area, see the section for the Call Stack panel.
Nothing is displayed on this panel during execution of a program. |
This section describes the following.
2.11.1.1 Change display format of values
2.11.1.2 Jump to the source line