You can move the caret to the address where the symbol is defined.
Click the button on the toolbar after moving the caret to the instruction which refers to the symbol.
Furthermore, click the button on the toolbar following the previous operation returns the caret to the instruction which refers to the symbol at previous caret is defined.