Follow the steps below to edit code.
Double-click the code to edit or select [Edit Code] from the context menu after moving the caret to the code to edit.
Use keyboard to directly edit the code.
Press the [Enter] key to write the code to the memory after editing.
If the edited instruction is invalid, the instruction is shown in red and will not be written to the memory.
When the code is written to the memory, the result of disassembling is also updated.