No events occur during step execution (including Return Out), as well as during program execution actuated by selecting [Go to Here] from the context menu. |
If the program to be debugged is downloaded again and the position at which some existing event is set happens, as a consequence of it, to be in the middle of an instruction, the relevant event needs to be reset. Here is the method for doing it. |
When debug information is available: |
When no debug information is available: |