With the address of the currently selected line referenced as a pointer, it is possible to have the corresponding place simultaneously displayed on other panels (the focus not moved).
Clicking the toolbar button starts a linked display on the Editor panel.
Clicking the toolbar button starts a linked display on the Disassemble panel.
Clicking the button again stops the linked display.
When you select [Jump to Source] or [Jump to Disassemble] from the context menu, the Editor panel or Disassemble panel opens, with the caret on it moved to the source line or address corresponding to the address of the currently selected line (the focus moved). |