Everything
2.12.1.1 Changing the form in which values are displayed

The display format of this panel can be changed using buttons below on the toolbar.

Notation

Shows the following buttons that change the form in which values are displayed.

 

AutoSelect

Displays values on this panel in per-variable predetermined notation (default).

Hexadecimal

Displays values on this panel in hexadecimal.

Decimal

Displays values on this panel in decimal.

Octal

Displays values on this panel in octal.

Binary

Displays values on this panel in binary.

Encoding

Shows the following buttons that change the encoding in which string variables are displayed.

 

ASCII

Displays string variables on this panel in ASCII code (default).

Shift_JIS

Displays string variables on this panel in Shift_JIS code.

EUC-JP

Displays string variables on this panel in EUC-JP code.

UTF-8

Displays string variables on this panel in UTF-8 code.

UTF-16 Big-Endian

Displays string variables on this panel in UTF-16 Big-Endian code.

UTF-16 Little-Endian

Displays string variables on this panel in UTF-16 Little-Endian code.

UTF-32 Big-Endian

Displays string variables on this panel in UTF-32 Big-Endian code.

UTF-32 Little-Endian

Displays string variables on this panel in UTF-32 Little-Endian code.