You can reset the CPU and start the execution of the program from the reset address.
Click the button on the debug toolbar.
When this operation is performed, the program continues to be executed until either of the following occurs:
The button has been clicked (see "2.10.1 Stop the program manually"). |
The PC has reached a breakpoint (see "2.10.2 Stop the program at the arbitrary position (breakpoint)"). |
A break event condition has been met (see "2.10.3 Stop the program at the arbitrary position (break event) [E1] [E20]" and "2.10.4 Stop the program with the access to variables/I/O registers"). |
Other break factors have occurred. |