Everything
1. GENERAL

This document describes internal error message, fatal error message, information message, choice message and warning message that CS+ outputs.

The message is output to Output panel or Message dialog box, etc..

Caution

When the E2 emulator (abbreviated name: E2) is used, please read references to "E1" in this manual as also meaning "E2".
When the E2 emulator Lite (abbreviated name: E2 Lite) is used, please read references to "E1" in this manual as also meaning "E2 Lite".
When the IE850A is used, please read references to "E1" in this manual as also meaning "IE850A".