Everything
B.1 Overview

The Python Console plug-in is a console tool using the IronPython language.

In addition to the functions and control statements supported by the IronPython language, you can also use CS+ Python functions added in order to control CS+.

The functions provided by CS+ are shown below.

 

-

On the Python Console panel, you can execute IronPython functions and control statements, and CS+ Python functions (see "B.3 CS+ Python Function/Class/Property/Event" and "2.1 Execute Python Functions").

-

When you start CS+ from the command line, you can specify and execute a script file (see "CS+ Project Operation").

-

When loading a project file, you can run a script you have prepared in advance (see "B.2 Related File").