Everything

Hook


This function registers a hook or callback function.

[Specification format]

Hook(scriptFile)

[Argument(s)]

Argument

Description

scriptFile

Specify the script file where the hook or callback function is defined.

[Return value]

None

[Detailed description]

-

This function loads scriptFile, and registers a hook or callback function in the script file.
There is no problem even if functions other than a hook or callback function are declared.
The hook or the callback function is registered when the script file is ended.

-

If Hook functions are declared, they are called after CS+ events occur.

Caution

Event processing by CS+ is not completed unless execution of the hook function completes or control returns to the calling program.

-

The types of hook function are shown below.
Note that hook functions do not take parameters.

Hook Function

Event

BeforeBuild

Before build

BeforeDownload

Before download

AfterDownload

After download

AfterCpuReset

After CPU reset

BeforeCpuRun

Before execute

AfterCpuStop

After break

AfterActionEvent

After action event (only Printf event)

AfterInterrupt

After acceptance of specified exception cause code

(the target is the exception cause code set in debugger.Interrupt.Notification)

AfterTimer

After occurrence of timer interrupt

(the target is the timer interrupt set in debugger.Interrupt.SetTimer)

Example

Sample script file

def BeforeDownload():
  # Processing you want to perform before the download

 

-

If callback functions are declared, they are called after CS+ events occur.

-

The callback function name is fixed to "pythonConsoleCallback".
The parameter of the callback function is the callback trigger.

Argument Value

Callback Trigger

10

After event registration

11

After event deletion

12

Before start of execution

13

After break

14

After CPU reset

18

After debug tool properties are changed

19

Before download

20

After memory or register is changed

21

After action event (only Printf event)

30

Before build

50

After occurrence of specified exception cause code

(after acceptance of exception cause code specified by debugger.Interrupt.Notification)

63

After period specified by XRunBreak or timer interrupt has elapsed

Caution 1.

Hook functions and callback functions are initialized by the following operations.

-

When a project file is loaded

-

When a new project file is created

-

When the active project is changed

-

When the debugging tool is switched

-

When Python is initialized

Caution 2.

Do not include a process that enters an infinite loop in hook functions and callback functions.

Caution 3.

Do not use the following functions in the hook functions and callback function.

debugger.ActionEvent, debugger.Breakpoint, debugger.Connect, 
debugger.Disconnect, debugger.Download, debugger.Erase, debugger.Go, 
debugger.Map, debugger.Next, debugger.Reset, debugger.ReturnOut, 
debugger.Run, debugger.Step, debugger.Stop

Caution 4.

It is not possible to call debugger.XRunBreak.Set or debugger.Interrupt.SetTimer with different conditions in the hook function (AfterTimer) and callback function (parameter: 63).

Example 1.

Do not make the following specifications in a hook function.

def AfterTimer():
  debugger.Interrupt.SetTimer(1, TimeType.Ms, True)
  debugger.XRunBreak.Set(1, TimeType.Ms, True)

Example 2.

Do not make the following specifications in a callback function.

def pythonConsoleCallback(Id):
  if Id = 63:
    debugger.XRunBreak.Delete()
    debugger.Interrupt.SetTimer(1, TimeType.Ms, True)
    debugger.XRunBreak.Set(1, TimeType.Ms, True)

Caution 5.

Use the following functions when the hook function is AfterTimer or AfterInterrupt and when the parameter of the callback function is 50 or 63.

debugger.Address, debugger.GetIORList, debugger.Interrupt, debugger.Memory, 
debugger.Register, debugger.Watch, debugger.XRunBreak

 

Note that debugger.Interrupt.SetTimer and debugger.XRunBreak cannot be used when the hook function is AfterTimer or when the parameter of the callback function is 63.

[Example of use]

>>>Hook("E:/TestFile/TestScript/testScriptFile2.py")