|
|
Option ( xxx) is not specified.
|
|
Make sure whether the configuration file input to an option is specified.
|
|
|
|
|
Make sure that the device file exists.
|
|
|
File name ( xxx) is duplicated.
|
|
|
Option ( xxx) needs parameters.
|
|
|
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
The parameters ( xxx) is illegal.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
|
|
Illegal parameters ( xxx).
|
|
|
|
|
The option ( xxx) is Illegal.
|
|
|
|
|
Illegal format is in command file.
|
|
Check the contents of a command file.
|
|
|
Path or file name is too long ( xxx).
|
|
|
File ( xxx) is not a supported file to convert.
|
|
|
A described device ( xxx) is not supported.
|
|
|
The size of the command ( xxx) file is too big.
|
|
|
Cannot open command file.
|
|
The specified command file could not be opened. Otherwise, the specified command file name is not valid.
|
|
Check whether the specified command file exists or whether the command file name is correct.
|
|
|
Usage:CF78V4 [@command file] [-i <SIT file> | -ni] [-dc <C header file> | -ndc] [-da <ASM header file> | -nda] [-V] [-help] <CF file>
Usage: CF78V4 [@command file] [-cpu <Name>] [-devpath=<Path>] [-i <SIT file> | -ni] [-dc <C header file> | -ndc] [-da <ASM header file> | -nda] [-V] [-help] <CF file>
|
|
Because the specified activation option is not correct, CF78V4 could not be executed.
|
|
Check the activation option.
|
|
|
Option ( xxx) is multiple defined.
|
|
Check the contents of a command file.
|
|
|
Output file names are the same ( xxx).
|
|
The output files (system information table file, system information header file (for C language) or system information header file (for assembly languages)) are specified with the same file name " xxx".
|
|
Check if the file names specified with the -i, -dc, and -da options are the same.
|
|
|
It is necessary to specify the device file in the case of outputing entry file.
|
|
Check the specified the output option of the entry file or the device file.
|
|
|
It failed to convert file ( xxx).
|
|
|
|
|
Check the description of the system configuration file.
|
|
|
Unknown device file format.
|
|
|
|
|
|
|
File ( xxx) cannot be read.
|
|
Check if the specified file exists. Alternatively, check whether the file name is correct or whether the file name is specified with the valid number of characters.
|
|
|
|
|
File ( xxx) could not be opened.
|
|
Check whether the file is write-enabled or whether the disk is full. Alternatively, check if the number of characters for the specified file name or output file name converted to an absolute path is valid.
|
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Cannot execute Preprocessor.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Check the pass of a preprocessor and the option.
|
|
Cannot execute Preprocessor ( xxx).
|
|
|
|
|
|
File name has already existed ( xxx).
|
|
|
|
|
The available memory is insufficient.
|
|
The available memory is insufficient.
The available memory is insufficient to analyze the activation option/command file or to analyze the system configuration file. Increase the memory capacity available for CF78V4 by quitting any applications that are not in use.
|
|
|
PEID(xxx) is not defined in the device file.
|
|
The specified PEID(xxx) is not defined in the device file.
|
|
Check the PE number as specified "-peid" option.
|
|
|
Cannot read xxx in the device file.
|
|
Cannot read the information "xxx" from the device file.
|
|
Renews the latest device file or reconsiders the specified option.
|
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
CF850V4 internal error ( xxx).
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Please contact your vendor or your Renesas Electronics overseas representative.
|
|
CF850MP internal error ( xxx).
|
|
Please contact your vendor or your Renesas Electronics overseas representative.
|