Everything

Create Sample Project

You generate the sample project as following steps.

 

Select the item including "Analysis_Tutorial" from [RL78] tab in [Open Sample Project], and click [GO] button.

After clicking [GO] button, select arbitrary folder,

then the sample project will be created in that folder.

 

Remark: The sample project for trying analysis features is prepared for 78K0, 78K0R, RL78, RX, V850 and RH850. This tutorial describes the case using the RL78 sample project (CS+ for CA,CX).

             78K0 :  78K0_KC2-L_Tutorial_Analysis

             78K0R :  78K0R_KG3_Tutorial_Analysis

             RL78 :  RL78_G13_Tutorial_Analysis_CA

             RX :  RX610_Tutorial_Analysis

             V850 :  V850ES_JG3-L_Tutorial_Analysis

RH850 : RH850_F1L_Tutorial_Analysis *

 

* It's the explanation only of the analysis for the followings in this tutorial.

- Execution Performance

- Performance

- Coverage