Everything

Connecting a Debugger and Downloading

3. Connecting E1

In this step, you perform on-chip debugging using E1.

 

Connecting E1 to RH850/F1L(176pin) board.

Connect E1 to the PC. "Found New Hardware Wizard" appears when E1 is connected for the first time. Select "Install software automatically" and install the USB driver following the instructions.