Displaying a Special Function Register (IOR)
Displaying IOR
In this section, you observe the value of the register that implements peripheral functions built in the microcontroller. First, let's make the panel float so that it is easier to view.
Select [IOR] from the [View] menu. |
This opens the IOR panel. |
Right-click on the title bar of the IOR panel and check the [Floating]. |
The IOR panel enters the floating state and it becomes easier to view. |