Everything

Termination Procedure

This section describes the termination procedure.

Click the Close button in the Main window.

This closes the Main window and exits CS+. If the environment is not saved, a window appears that prompts you to select whether or not to save it, so follow the instructions.

 

Tip

Saving the development environment (project saving function and packing function)

CS+ provides two functions (project saving function and packing function) for saving the development environment. Each of these functions is used to save the content shown in the figure below. You can choose to use either saving function depending on the development phase.