Everything

Overview of the Program

This section describes an overview of the sample program and RH850/F1L(176pin) board.

 

1. Overview of the Program

The program is simple program which causes LEDs flash alternately.

 

 

 

 


LEDs flash alternately

 

2. Overview of RH850/F1L(176pin) board

The following is an overview of RH850/F1L(176pin) board.

 

 

 

Evaluation LED1-4 : Lights in yellow when the P8_4 to P8_7 is LOW.

14pin connector   : Used for on-chip debugging and writing.