Everything

Manipulating Windows

2. Automatic hiding

By clicking the Pin icon on the title bar of each panel, you can easily change the setting that determines whether or not to hide the panel automatically. By hiding the panel not necessary for operation, you can use the screen more effectively.

(a) Hiding the panel automatically (example: Project Tree)

Click the Pin icon in the Project Tree.

The Project Tree automatically disappears and the tab representing it appears.

 

 (b) Displaying the hidden panel (example: Project Tree)

 Place the pointer on the [Project Tree] tab.

 

The Project Tree slides out.

 

Tip

Locations to hide the panels

You can hide the panel in three locations: one to the left of the window, one to the right of the window and one below the window. You can also hide multiple panels in the same location.