Everything

Generating code

4. Generating code

When the configuration of the functions to be used is completed, generate the program.

 

The program is generated by clicking the [Generate Code] button on the toolbar.

The generated program is displayed in the Project Tree.

 

Tip

Before generating code

You can confirm the content of the program that will be generated without actually generating the code. This is called a "code generator preview" function. Double-click  the source file from [Code Generator (Design Tool)] > [Code Preview] in the Project Tree.