| Plug-in Manager dialog box | 
This dialog box is used to set the plug-ins to be read in when this product is started.
| 
Caution | The settings in this dialog box are effective from the next time this product is started. | 
| 
Figure A.54 | Plug-in Manager Dialog Box | 
 
The following items are explained here.
[How to open]
| 
- | From the [Tool] menu, select [Plug-in Setting...]. | 
[Description of each area]
By selecting a tab, the plug-ins displayed in the plug-in list area are switched.
This dialog box has the following tabs:
Select the plug-ins read when this product is started with check boxes.
For details of displayed items/setting method, see the description of each tab.
| 
Remark | You can select all check boxes or clear them by clicking buttons displayed on the upper left of this area. | 
| 
  | 
Selects all check boxes. | 
| 
  | 
Clears all check boxes. | 
| 
  | 
Toggles all check boxes. | 
[Function buttons]
|  |  | 
| 
OK | 
Applies all setting and closes this dialog box. | 
| 
Cancel | 
Cancels the designated condition and closes the dialog box. | 
| 
Help | 
Displays the help of this dialog box. |