Everything
 

[Additional Function] tab


This tab is used to set the plug-ins other than build tool and debug tool plug-ins to be read in when this product is started (plug-ins present in the Plugins folder of this product).

Caution

The plug-ins except for the Editor panel are disabled on this tab after default installation.
To use each plug-in, enable it on this tab and then restart CS+.

Figure A.56

Plug-in Manager Dialog Box: [Additional Function] Tab

 

The following items are explained here.

[How to open]

-

From the [Tool] menu, select [Plug-in Setting...].

[Description of each area]

(1)

Plug-in list area

This area shows a list of the plug-ins other than build tool and debug tool plug-ins installed in this product (plug-ins present in the Plugins folder of this product), in the following format.

Module Name

Shows the plug-in module names.

The plug-ins read in when this product is started are selected with check boxes.

Description

Shows a simple description of the plug-in.

Remark 1.

The Editor panel plug-in cannot be removed from the list of those read in, and so the display is grayed out.

Remark 2.

When this product is started from the command line, plug-ins below the Plugins folder specified with the /np option do not appear in this area. When the /npall option is specified, plug-ins below the Plugins folder are not read in, and thus nothing appears in this area.
See "2.13 Manipulate CS+ on the Command Line" for details about the /np and /npall options.

[Function buttons]

Button

Function

OK

Applies all setting and closes this dialog box.

Cancel

Cancels the designated condition and closes the dialog box.

Help

Displays the help of this dialog box.