You can import the build options of other project to the current project.
On the project tree, select the Build tool node, and then select [Import Build Options...] from the context menu. The following message dialog box will open.
 
Click [Yes] in the dialog box. The Import Build Options dialog box will open.
 
In the dialog box, select the target project file for importing the build options and click the [Open] button.
The build options of the selected project file are imported to the current project.
| The target build options for importing are only the general options set in the properties of the build tool. | 
| All the build modes of the import target are imported. |