You can save the project file and all the files being edited.
From the [File] or [Project] menu, select [Save All], the project file is overwritten with the current settings information and all files being edited are saved.
Figure 2.99 | [Save All] Item |