2.1 Installing License Manager
Install the license manager which is included in the installer for the CS+ IDE, or with a package for a stand-alone language tool.
The preparing for installation window automatically appears. If this does not happen, double-click on “Setup.exe” in the root directory of the CD.
Caution | The floating license client setup must be conducted with administrator privileges. |