On the Analysis Result panel, you can zoom in or out the period of analysis information to be displayed as a processing program execution transition state or a real-time OS resource usage status, in the Analysis information diagram area.
The period of Analysis information diagram area is zoomed in or out by dragging Zoom in or out slider of execution transition display or pressing Zoom in button of execution transition display and Zoom out button of execution transition display.