When the message number type is information, the information types are classified as follows.
Table 4.2  | Information Types  | 
 
| 
 | 
 | 
| 
 
Change 
 | 
 
Changes were made in the program so that it can be handled by the CC-RL. 
 | 
| 
 
Insert 
 | 
 
Additions were made in the program so that it can be handled by the CC-RL. 
 | 
| 
 
Delete 
 | 
 
Some descriptions were deleted because they are not necessary in the CC-RL. 
 | 
| 
 
Info 
 | 
 
Conversion may not be sufficient in some cases because of the difference between the CA78K0R and CC-RL specifications. 
Each case should be confirmed individually. 
 |