Reads the results of A/D conversion (8 bits; most significant 8 bits of 10-bit resolution).
[Syntax]
#include “r_cg_macrodriver.h”
void R_ADC_Get_Result ( uint8_t * const buffer);
[Argument(s)]
| 
       I/O  | 
    
       Argument  | 
    
       Description  | 
| 
       O  | 
    
       Uint8_t * const buffer;  | 
    
       Pointer to area in which to store the results of A/D conversion  | 
Remark Below is an example of the results of A/D conversion to be stored in buffer.
![]()  | 
[Return value]
None.